{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to select the proper fuse rated current for my transformer protection by RM6 switch-fuse unit?
Below selection table gives the fuse rated current based on network (service) voltage and transformer rated power:



Important notes:
  1. Correct operation of the RM6 is not guaranteed when using fuses from other manufacturers,
  2. Fuse rating given in A, no overload, – 25°C < Temperature < 40°C),
  3. Fuse type considers: Fusarc CF and SIBA (1) (General case, IEC 60282-1 standard, IEC 62271-105 (to replace IEC 60420) and DIN 43625 standard),
Fuses dimensions (Fusarc CF):


Schneider Electric Saudi Arabia