{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

NetBotz 750 | How do I connect serially?

Issue:
How do I serially connect to the NetBotz 750?

Product Line:
NetBotz version 5.X

Environment:
NetBotz v5.X

Cause:
Serial parameters and drivers are required to establish a serial connection between a computer and the NetBotz appliance.

Resolution:

The NetBotz 750 uses the following serial parameters:
- Baud Rate: 115200
- Data Bits: 8
- Parity: None
- Stop Bits: 1
- Flow Control: None

To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password.

If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:

Serial port driver - Silcon Labs CP2103
https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: