{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the optional control power transformer part number used in the enclosed ATS22 with the B10 mod?
Issue:
Transformer used in the enclosed ATS22 with the B10 Mod.

Product Line:
B10 Mod used in the Enclosed ATS22

Environment:
All

Cause:
Transformer part number.

Resolution:
When the B10 option is selected, transformer# 9070TF300D1 will be included in this enclosure.  If a transformer larger than this is needed, I would recommend contacting our drives quotes group. They provide support for custom enclosed drive and soft starter applications

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: