{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider offer HP rated relays for hazardous location?
Issue:
Class 1 Div 2 HP rated Relay

Product Line:
General Purpose Relays

Environment:
Legacy General Purpose Relays

Resolution:
782H SE Legacy Relays are rated for 1/10HP @120 or 240
750H SE Legacy Relays are rated for 1/2HP @240V, and 1/3HP @120V
8501R hermetically sealed relays has no HP ratings

Schneider Electric Saudi Arabia