{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
VIP 400 relay is showing Status LED Flashing and MITOP FAULT ALARM Screen.What is the solution ?
Lighting up of the LED (flashing) and display of the MITOP FAULT alarm indicate that the VIP has
detected a fault in the Mitop trip unit connection circuit. In this case, the VIP does not go into the fail-safe
position and remains operational.

The VIP remains operational. Check the wired connection between the VIP and the Mitop trip unit.


Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.