{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What could cause the Current Limitation function of the ATV71 series drive to not limit the motor current?

Issue:
Why would the Current Limitation function of the ATV71 series drive not limit running motor current.

Product Line:
ATV71 series drives.

Environment:
All

Cause:
Current Limitation has not been configured for the motor

Resolution:
When Current Limitation (CLI) is set to a value lower than the no-load current of the motor, the function becomes inactive.  Otherwise there would be no way to turn the motor.   Ensure that the Motor Rated Current and Motor Thermal Current settings were configured to match the motor's nameplate.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: