Search FAQs
What CanOpen Connector type and cable can I use for the Lexium LXM15 servo drive?
For a cable + connector for Lexium 15 canopen interface, it is necessary either to use old adapter AM02CA001V000 (see pages i attachment, but bear in mind that old adapter is no longer commercialized) or to make canopen connector manually by buying standard subD-9 and solder dedicated canopen pins (CAN_H, CAN_L and GND).
The last device on bus must have termination, that consists of 120 Ohms resistor between Can_H and Can_L signals.
The last device on bus must have termination, that consists of 120 Ohms resistor between Can_H and Can_L signals.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: