{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause a Load Slipping (ANF) fault on an ATV340 series drive?
Issue:
ATV340 drive shuts down with ANF Load Slipping Fault.

Product Line:
ATV340 series

Environment:
In applications using an encoder

Cause:
The difference between the output frequency and the speed feedback is not correct.

Resolution:
  • Confirm the drive rating according to the application (motor, load, and so on.)
  • Verify the motor, gain, and stability parameters.
  • Add a braking resistor.
  • Verify the mechanical coupling and wiring of the encoder.

If the torque control function is used and if the encoder is assigned to speed feedback:
  • Set [Load slip detection] Sdd = [No] no.
  • Set both [Positive deadband] dbp and [Negative deadband] dbn to a value less than 10% of the nominal motor frequency.

Schneider Electric Saudi Arabia