{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many cables can be connected to the 04456 connection plate?
The distance between two consecutive connection plates on the 04456 is 64 / 65mm:

Each connection plate is prepared for the connection of maximum 8 cables (4 on each face of a connector plate).


It's the responsibility of the panel builder and sub-contractor to check creepage distance and more specifically clearance distance of connections on the connector plates: see IEC61439-1, for Ui =1000V the clearance distance must be greater or equal to 14 mm.

Schneider Electric Saudi Arabia