Issue:
ATV320 obsolescence
Product Line:
Altivar 320
Environment:
All model numbers, all serial numbers
Cause:
Obsolescence documentation
Resolution:
The ATV320 is not obsolete.
It is a currently marketed product line, introduced in 2016.
The ATV320 is the functional replacement for the ATV32 and the ATV312, both obsoleted in 2017.
updated Feb 2022
ATV320 obsolescence
Product Line:
Altivar 320
Environment:
All model numbers, all serial numbers
Cause:
Obsolescence documentation
Resolution:
The ATV320 is not obsolete.
It is a currently marketed product line, introduced in 2016.
The ATV320 is the functional replacement for the ATV32 and the ATV312, both obsoleted in 2017.
updated Feb 2022
Released for:Schneider Electric Saudi Arabia