Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate necessary Air flow for cabinet cooling using Altivar variable speed drives heat dissipation.

Article available in these languages: Czech

The most precise method for calculating heating/cooling system for cabinet is to use dedicated software for cabinet thermal calculation. ProClima software is available on schneider web.
Besides that, it is also possible to calculation required fan flow manually, though certain inaccuracy will be caused by not-knowing the amount of heat dissipated by cabinet walls.
Manual calculation can be done based on following known (input) data:
- Total heat produced inside cabinet (W) - Ptotal
- Max ambient temperature (of cooling air) (deg.C) - Tomax
- Max allowed temp inside cabinet (deg.C)  - Timax
- Parameters of cooling air (specific thermal capacity c, density ro)

Min air flow is calculated as :

Qmin=
Ptotal /(ro*c*(Timax-Tomax))

Where Qmin is in m3/s
Ptotal in kW
ro in kg/m3
c in kJ/(kg.K)
Tomax, Timax in degrees celsius

To get value of flow in m3/h, multiply result by 3600.
Qmin (m3/h) = 3600 * Qmin (m3/s)

In case of air:
ro=1.1kg/m3 (at 40 degrees Celsius)
c= aprox 1kJ/kgK

Example:
Devices inside cabinet produce total heat losses 560W (Ptotal=0.56kW)
Max operational temperature for devices inside cabinet is 50 degrees celsius (Timax=50 C)
Temperature of cooling air (ro=1.1kg/m^3, c=1kJ/KgK) never exceeds 25 degrees celsius (Tomax=25 C)

Min amount of air is then:

Q [m3/s] =0.56 kW /(1.1 kg/m3 * 1kJ/kgK * (50-25)K) = 0.56kW / 27.5 kJ/m3 = 0.020 m3/s = 20 liters/s
Q [m3/h] = 3600 * Q [m3/s] = 3600 * 0.020 = 73 m3/h

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.