{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What causes an OSF, Mains Overvoltage fault on the ATV340 drive?
Issue:
Possible causes of mains overvoltage fault (OSF) on the ATV340 drive.

Product Line:
Altivar 340

Environment:
All

Cause:
N/A

Resolution:
A mains overvoltage fault can be caused by a number of reasons:
  • Standard high voltage potential on the drive line terminals L1, L2, and L3.  (Supply voltage is too high)
  • Measure voltage phase to phase to confirm that the voltage supplied does not surpass the drive's rating.
  • Power quality issues in the line supply side of the drive.
  • Spikes or poor power quality can over charge the drives DC bus (PA and PC).  These can be hard to pinpoint as the spikes will not be detected by your standard fluke voltage meter.
  • Should be measuring ~1.41 X line voltage coming in.  If it reads higher then that would indicate that the drive is picking up spikes.

Schneider Electric Saudi Arabia