{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is a FLU status at the top left of the HMI display of ATV71?

Issue:
ATV71 showing FLU on the top left corner of the HMI.

Product Line:
ATV71

Environment:
All serial numbers

Cause:
Customer wanted to know what is the FLU code on the keypad.

Resolution:
FLU is a status of the drive meaning Motor fluxing in progress.  Under 1.3 Settings in the Drive Menu, Motor Fluxing can be set to FnC (not cont), FCt (Continuous) or Fno (No or Function inactive).

• In [Continuous] (FCt) mode, the drive automatically builds up flux when it is powered up.

• In [Not cont.] (FnC) mode, fluxing occurs when the motor starts up.

CAUTION

Check that the motor will withstand this current without overheating.

Failure to follow this instruction can result in equipment damage.

Schneider Electric Saudi Arabia