{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Network Shutdown does not proceed with VM Startup after powering on the vCenter Server VM
Issue:
PowerChute Network Shutdown does not proceed with VM Startup after powering on the vCenter Server VM. PowerChute shows an event log entry “Attempting to start vCenter Server VM <VM Name>” but does not proceed to power on VMs.

Product Line:
PowerChute Network Shutdown v4.2, v4.3, v4.4

Environment:
PowerChute Network Shutdown configured with VMware


Cause:
This can occur when some vCenter Services are unable to start.

Solution:

Connect to the vCenter Server VM and check the status of vCenter Services. Manually start services that have not started.
  • On Windows, the services.msc console can be used.
  • On Linux, execute the following command:
service-control --status -all

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.