{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is the value of motor torque (OTR) obtained in the ATV320 drive?
Issue:
Needs to know the motor torque (OTR) on an ATV320 drive

Product Line:
ATV320

Environment:
All

Cause:
Wants to know how motor torque monitoring is achieved. Is it measured or estimated

Resolution:
On ATV320, this parameter will be estimated (the torque is estimated based on motor current measured).
The torque of motor is not measured by the drive. It is calculated from the measurement of motor
current.
OTR = (Iq / Iqn) * (PhirdRef / Phirn) in %
With: Iq : Current torque provided by the command to drive motor
PhirdRef : Flux provide by the command to drive motor
Iqn : Nominal Current torque compute with the motor name plate
Phirn : Nominal flux of the motor

Schneider Electric Saudi Arabia