{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the NSYAEFPFPTD accessory to the NSYPTDS* flange kit?
Issue:
NSYAEFPFPTD accessory in the NSYPTDS* flange kit.

Product Line:
Process drives

Environment:
N/A

Cause:
Option or required?

Resolution:
When a Process drive is flange mounted into a wall mounted enclosure, the heatsink extends out the back.  Space is required between the enclosure and wall to accommodate the heatsink and airflow.  The NSYAEFPFPTD is a bracket kit to extend the enclosure away from the wall.  The bracket can provide the space for the NSYPTDS1, NSYPTDS2, and NSYPTDS3 flanged drives.
See the attached file.

Schneider Electric Saudi Arabia

Attachment(s)
Flange mtd brkt NSYAEFPFPTD NHA3487201_00 Process.pdf [411.19 KB]