{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to remotely control (open/close) circuit breakers using IFE switchboard server and a browser. Discovering devices, creating a device list and enabling application control.

Issue:
This FAQ focuses in on the IFE switchboard server setup to remotely control open and close a circuit breaker using the embedded webpage, Powerview. Namely how to discover devices, create a device list and how to enable application control. However, one of the attachments is an example of what other components are needed, like MX-Com and XF-Com communicating coils, BCM, IFE Server, how to wire the communications coils etc.

Product Line:
Circuit Breakers

Environment:
Masterpact NT, NW and MTZ

Resolution:
Summary of Activity:
• Install MX-COM and XF-COM coils
• Install communications wire harness between coils and BCM
• Modify MX-COM and XF-COM input power wiring
• Install one IFE switchboard Server in place of one existing standard IFE, or add the IFE switchboard server in the ethernet daisy change with the IFE's
• Configure IFE switchboard server, namely discovering devices, creating a device list and enabling application control

See attached documents for example diagrams and specific instructions on how to discover devices, create a device list and how to enable application control.

Schneider Electric Saudi Arabia

Attachment(s)

FAQ Example IFE Swbd Server Network Diagram.pdfFAQ Example IFE Swbd Server Network Diagram.pdf [281.17 KB]
IFE Device Discovery Guide.pdfIFE Device Discovery Guide.pdf [927.59 KB]
FAQ Browser communication system for controlling breakers IFE switchboard server.pdfFAQ Browser communication system for controlling breakers IFE switchboard server.pdf [324.41 KB]
Enable Application Control pages from IFE user guide 1040IB1401-05 R07-2017.pdfEnable Application Control pages from IFE user guide 1040IB1401-05 R07-2017.pdf [106.38 KB]