{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Firmware Links for 140CPU43412A Update from Concept to Unity System
To update your 140CPU43412A from Concept to Unity, first of all, please make sure the PV version is greater or equal to 04(PV can be seen from the top front of the CPU module), otherwise, it is not possible to update.

If you have the PV greater or equal to 04 but less then 16, please use the following intermediate OS and the last firmware:

140CPU43412U Intermediate OS (PV of module less than 16)

Quantum 140CPU43412U PV<16 Last Firmware


If you have the PV greater or equal to 16, please use the following intermediate OS and last firmware:

140CPU43412U Intermediate OS ( PV of module greater or equal to 16 )

Quantum 140CPU43412U PV>=16 Last Firmware

Also, using Modbus communication for the firmware update is slow, Modbus plus is much faster. If you don't have the MB+ cable, another option is to send the part to our repair center for them to update the firmware for you.

For the Modbus communication cable, if you need to make a cable by yourself, please refer to attached pin out for details.

Please refer to the following link for the update procedure:
https://www.se.com/ww/en/download/document/EIO0000000064/

Schneider Electric Saudi Arabia

Attachment(s)
990NAA26320 Cable pinout.docx [17.87 KB]