{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the operating time of ground fault protection devices defined in the UL 1053 standard?

The UL 1053 standard defines in Table 22.1 the operating time of the ground fault protection devices:
Ground-fault current (A)Time (s)
85% of pickup currentShall not trip
115% of pickup currentUltimately
150% of pickup current2
250% of pickup current1

Schneider Electric Saudi Arabia