Is EMC plate included in Altivar ATV320 variable speed drive delivery?
Yes, the EMC plate is delivered together with the Altivar ATV320, but it is not mounted on the drive. The screws for the EMC plate installation are also included in the Altivar package.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Altivar Machine ATV320
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.