Issue:
Is it possible to add a 2nd analog output on the ATV340 Drive?
Product Line:
ATV340
Environment:
All
Cause:
Customer needs a second analog output. Looking for an I/O expansion module
Resolution:
No. There are only 2 I/O expansion modules for the ATV340 drive. The VW3A3203 has 6 digital inputs, 2 digital outputs, and 2 analog inputs, and the VW3A3204 has 3 relay outputs.
Is it possible to add a 2nd analog output on the ATV340 Drive?
Product Line:
ATV340
Environment:
All
Cause:
Customer needs a second analog output. Looking for an I/O expansion module
Resolution:
No. There are only 2 I/O expansion modules for the ATV340 drive. The VW3A3203 has 6 digital inputs, 2 digital outputs, and 2 analog inputs, and the VW3A3204 has 3 relay outputs.
Released for:Schneider Electric Saudi Arabia