{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What's the difference between Power Supply (P/N MTN693004 ) and KNX Power Supply (P/N MTN684064)?

1. MTN693004 is a normal 24Vdc power supply (it is not a KNX power supply) that can provide ONLY power to the devices connected to it.
2. MTN684032, MTN684064, MTN683832 and MTN683890 are real 24Vdc "KNX" power supplies that not only provide POWER through their wires to the connected KNX devices but also provide COMMUNICATOIN between these KNX devices through the bus channel.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: