{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to display the Target Name and other system information during Vijeo Designer Runtime?
Issue:
Looking for a way to show some useful information regarding the application running on the HMI during runtime operation.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, we provide an operation that is able to retrieve the target name, project name, IP address, DRAM Usage and other useful information of a project and write the values to Vijeo Designer variables. To do so, follow this procedure:

For this example, we will use the Target Name as our Parameter. The process is the same for the others, except you might need to use an INT variable for DRAM Usage for example. Also, if you want a periodic update, you should use a Periodic Action rather than an On Startup Action.

1) Create a new Global Action
2) Set the Trigger Type to "Event"
3) Set to Trigger Event to "On Startup"
4) Press Next
5) Set Operation to "Information"
6) Set Information Type to "Target Name"
7) Set Destination to a String Variable of your choice.
8) Press Add
9) Press Finish
10) On a panel, draw a String display and assign the String variable to it.

Schneider Electric Saudi Arabia