{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV320 How do I achieve the fastest stop?

Article available in these languages: Czech

Issue:
How to get the "fastest" possible stop with an ATV320?

Product Line:
ATV320

Environment:
All serial numbers

Cause:
Need a fastest stop time.

Resolution:
With a "beefy" brake resistor that can handle the load.
Go to Full, then Fun menu:
Ramp: brA ( Dec ramp adapt). set to "no"

Then go to Stt [Type of stop]- Set to Fast stop
And Ramp divider ( dcF)- set to 0.

Schneider Electric Saudi Arabia