Search FAQs
How can you set, change or remove the password on the Process drives using the Somove software?
Issue:
Customer wants to reset the password using Somove software.
Product Line:
Somove and Process Drive ATV630 and ATV930.
Environment:
All
Cause:
Reset the password using Somove.
Resolution:
On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.
1. To set the password:
2. To change the password:
3. To remove password:
4. Protecting the SoMove file can be done by File/Project properties:
Customer wants to reset the password using Somove software.
Product Line:
Somove and Process Drive ATV630 and ATV930.
Environment:
All
Cause:
Reset the password using Somove.
Resolution:
On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.
1. To set the password:
2. To change the password:
3. To remove password:
4. Protecting the SoMove file can be done by File/Project properties:
Released for:Schneider Electric Saudi Arabia
Explore more
Product:
Explore more
Product: