{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In need of none or odd parity setting on the Link150 when Modbus ASCII is used

Issue:

The user may require a specific parity setting on the Link150 (EGX150) when the transmission mode has been set to Modbus ASCII

Product Line:

Link150 (EGX150)

Resolution:

When the transmission mode is set to Modbus ASCII, the parity of the serial port is limited to EVEN. Unfortunately, parity cannot be adjusted to none or odd.

Schneider Electric Saudi Arabia