{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an ATV320 be used for Synchronous reluctance motors?

Article available in these languages: Spanish

Issue:
ATV320 with Synchronous reluctance motors.

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
NA

Resolution:
No, the ATV320 is not designed for reluctance type synchronous motors.  Only ATV600/900 series and ATV340 drives can be used with reluctance motors. These drives have the control law dedicated to run this kind of motor.

Schneider Electric Saudi Arabia