Regarding the functions, ATV340 is more machine oriented, has built in encoder card and few functions are different.
ATV900 is process oriented and has few pump functions (for pumps other than those with quadratic torque), for example it offers backspin control, sleep-wake up.
ATV340 has positioning by sensors - typical for machines. Also support synchronous motors in close loop.
Ethernet is built-in all ATV9xx but only in ATV340..E
ATV900 has wider accessories than ATV340, especially for output filters when ATV900 is placed far from the motor. ATV340 in machine is not supposed to be far from the motor.
Otherwise, today 95% of the functions are identical.
Released for: Schneider Electric Saudi Arabia




Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.