Issue:
Customer wants to control an ATV12 series drive via the remote keypad VW3A1106 / 1107
Product line:
ATV12
Environment:
All ATV12 models where the VW3A1106 / 1107 keypad will be used.
Cause:
information unavailable in current literature.
Resolution:
Use the remote keypad and start with the display at rdy
Press the ENT button and use the down arrow to get to COnF.
Press ENT then scroll to FULL.
Press ENT then scroll to CtL.
Press ENT then scroll to Fr1.
Press ENT and scroll to LCC.
Press Enter, then press ESC until back to RDY.
The drive is now configured for start, stop, and speed control from the keypad.
The Run and Stop buttons on the keypad are used to start and stop the motor.
To change the speed, press ENT from the default screen (normally shows rdy when not running or the output frequency when it is running) to get to rEF.
Press ENT a second time to show the current frequency setpoint and use the UP and Down Arrows to adjust to a different value.
Customer wants to control an ATV12 series drive via the remote keypad VW3A1106 / 1107
Product line:
ATV12
Environment:
All ATV12 models where the VW3A1106 / 1107 keypad will be used.
Cause:
information unavailable in current literature.
Resolution:
Use the remote keypad and start with the display at rdy
Press the ENT button and use the down arrow to get to COnF.
Press ENT then scroll to FULL.
Press ENT then scroll to CtL.
Press ENT then scroll to Fr1.
Press ENT and scroll to LCC.
Press Enter, then press ESC until back to RDY.
The drive is now configured for start, stop, and speed control from the keypad.
The Run and Stop buttons on the keypad are used to start and stop the motor.
To change the speed, press ENT from the default screen (normally shows rdy when not running or the output frequency when it is running) to get to rEF.
Press ENT a second time to show the current frequency setpoint and use the UP and Down Arrows to adjust to a different value.
Released for:Schneider Electric Saudi Arabia