{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the NetShelter SX block electromagnetic (EM) or radio frequency (RF) interference?
Issue:
A customer is looking for a cabinet that provides EMI and/or RFI protection.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Excess EMI or RFI can interfere with the equipment installed in the cabinet.

Resolution:

The NetShelter SX cabinets have not been tested for EMI/RFI. The SX cabinets were not specifically designed as EMI/RFI cabinets.

Schneider Electric Saudi Arabia