1.Issue
IPC HMIPSOS552D1801 built-in Win10 operating system’s screen resolution cannot set to 1280*800 to meet Vijeo Designer’s requirement.2.Resolution
For some HMIPSOS5521D1801 IPC’s built-in Win10 operating system, the required graphic drivers are not installed in the factory. Customers need to download from official website and install on the IPCs. The download link is as follows.https://www.se.com/ww/en/download/document/Magelis+S-Panel+PC+HMIPSO+-+drivers+for+Win10/
3.FAQ applicable conditions
FAQ also applies to other Magelis S-Panel PCs.Released for:Schneider Electric Saudi Arabia