Search FAQs
How to deal with unexpected Short/Close status of IO digital output during Installation of IO Module (LV434063)?
Possible cause:
Shock and vibration on bistable relays during transit
Affected product:
IO Module (LV434063) with firmware version 3.3.11 and earlier.
Solution 1:
Upgrade IO module to v003.004.005 using EcoStruxure Power Commission (v2.12.0.2007 and later).
Solution 2:
FORCE digital outputs to 1, then FORCE to 0, and then UNFORCE.
Procedure
• Using EcoStruxure Power Commission
- Open EcoStruxure Power Commission application software and discover your gateway device.
- Click CONNECT.
- Select Device Check Up tab and go to I/O Status tab.
- Select the respective I/O Module (I/O Module 1 or I/O Module 2) on the left side pane.
- Select the check boxes to select all three digital outputs of I/O module.
- Digital Output 1
- Digital Output 2
- Digital Output 3
- Click FORCE TO 1.
- You will be prompted to enter the password to perform this operation.
- Enter the password and click CONTINUE.
- A “Success” message is displayed on the Test Result column.
- Select all three digital outputs of same I/O module again.
- Click FORCE TO 0.
- You will be prompted to enter the password again.
- Enter the password and click CONTINUE.
- A “Success” message is displayed on the Test Result column.
- Select all three digital outputs of same I/O module again.
- Click UNFORCE.
- You will be prompted to enter the password again.
- Enter the password and click CONTINUE.
- A “Success” message is displayed on the Test Result column.
- Refer to the snapshot (attached below) of the EcoStruxure Power Commission.
• Using FDM121 Display Module
- Connect FDM121 display modue.
- Navigate to Main menu and select Services.
- Navigate to I/O Module and select the module (I/O Module 1 or I/O Module 2).
- Navigate to Force.
- Press OK on Force and navigate to O1, O2, or O3.
- Select O1 and press OK.
- Select Force to 1 and press OK.
- Select YES and press OK.
Result: You will be prompted to enter the password. - Enter the password and press OK.
Result: The status changes to 1F, which can be seen in front of O1 in the same screen or in Status menu. - Select Force to 0 and press OK.
- Select YES and press OK.
- You will be prompted to enter the password.
- Enter the password and press OK.
Result: The status changes to 0F, which can be seen in front of O1 in the same screen or in Status menu. - Select UnForce and press OK.
- Repeat steps 6 through 14 to change the status of other digital outputs (O2 and O3) to complete Force to 1, Force to 0, and then UnForce.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: