{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is SSF code on the ATV320 drives?
Issue:
Altivar 320 drive is showing SSF and the motor will not run.

Product line:
Altivar 320, Altivar Machine

Environment:
All model numbers, all serial numbers

Cause:
Torque Limitation

Resolution:
SSF means the drive has reach the Torque Limit fault setting.  This parameter is not enabled by default on the drive.
To disable go to CONF > FULL > FLT > TLD > SSD and change the setting to 'no'.

Schneider Electric Saudi Arabia