{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can be done if a Flashing 'E' can't be cleared on an ATV212 (or S-Flex) with power cycle or fault reset input?
Issue:
Getting a Flashing 'E and can't be cleared on an ATV212 (or S-Flex) with power cycle or fault reset input.

Product Line:
Altivar 212

Environment:
All

Cause:
Flashing 'E' on the display doesn't clear with a power cycle or fault reset input activation as it should

Resolution:
Normally, a flashing 'E' should be cleared by cycling power to the drive or by activating a logic input assigned to fault reset.
However, there have been cases where neither of these remedies cleared the flashing 'E'.
In these situations try keeping the fault reset logic input activated (maintain 24V on the input) while cycling power to the drive.
Make sure the drive's display goes all the way out before restoring line voltage to the drive.
When the drive powers back up, deactivate the fault reset input.
This should clear the flashing 'E'.

Schneider Electric Saudi Arabia