Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to flash the firmware of the LXM28 drive
Issue:
How to flash the firmware of the LXM28 drive

Product Line:
LXM28
Lexium 28

Resolution:
To flash the LXM28 drive firmware, the following are needed:
- Latest firmware file (currently V1.70.8). This is a file with the extension *.i00 and can be requested from technical support.
- Firmware Update Tool (latest version is 1.0.2.8) and can also be requested from technical support
- USB to RJ45 cable, part # TCSMCNAM3M002P

> Power the LXM28 drive
>
Connect the USB-RJ45 cable
> Launch the Firmware Update Tool
> Enter the COM port assigned by Windows to the cable
> Browse the firmware in the "Firmware Path"
> Click on Connect - If successful, this should bring up the drive model and version
> Click on Start and wait

The Flash tool is attached herewith.

Schneider Electric Saudi Arabia

Attachment(s)
Fw Update Tool_1028.zip [188.79 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.