{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to read the version of VW3A1111 display?
Fw version used in VW3A111 HMI can be read from:
- from HMI directly during powering up the drive where HMI is placed, see picture attached. 1.2 IE 39 is fw version in my case
- by reading the content of keypad_id.bin file present in HMI, see attached file. The file can be read when you connect HMI to PC via usb. The file is in folder KPCONF.

Schneider Electric Saudi Arabia

Attachment(s)
HMI1.jpg [533.23 KB]
HMI2.jpg [72.76 KB]