{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212 Programming & Wiring an E-Stop

Article available in these languages: Spanish

Issue:
Programming & Wiring an E-Stop for the ATV212.

Product Line:
ATV212

Environment:
All model numbers, all serial numbers

Cause:
n/a

Resolution:
Consider using a logic input that is assigned as run permissive. If the input drops out, the VFD will remove output power to the motor.
Wire the normally closed E-stop contact between  R and P24.
Program F110 = 0, F112 = 1.
The VFD will display OFF to indicate that a run permissive is not enabled.

Schneider Electric Saudi Arabia