Search FAQs
How many SmartX living space sensors can be connected to SmartX IP controller?
Issue:
What is the maximum number of SmartX Sensors can be connected to a SmartX IP controller (MP-C, MP-V, RP-C).
Product Line:
EcoStruxure Building Operation, SmartX living space sensors
Resolution:
SmartX Sensors are a family of living space sensors designed for SmartX IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the SmartX IP controller.
The maximum number of SmartX Sensors you can connect to a SmartX IP controller depends on the selected combination of cover and sensor base types. The limit also depends on whether an eCommission Bluetooth Adapter is connected to the sensor.
You can combine sensor bases and covers as follows:
• Blank covers: Up to four sensors of any combination of sensor base types
• 3-button and touchscreen covers:
– Up to two sensor bases with CO2 option
– Up to four sensor bases without CO2 option
• SmartX LCD temperature sensors: Up to four sensors are supported
What is the maximum number of SmartX Sensors can be connected to a SmartX IP controller (MP-C, MP-V, RP-C).
Product Line:
EcoStruxure Building Operation, SmartX living space sensors
Resolution:
SmartX Sensors are a family of living space sensors designed for SmartX IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the SmartX IP controller.
The maximum number of SmartX Sensors you can connect to a SmartX IP controller depends on the selected combination of cover and sensor base types. The limit also depends on whether an eCommission Bluetooth Adapter is connected to the sensor.
You can combine sensor bases and covers as follows:
• Blank covers: Up to four sensors of any combination of sensor base types
• 3-button and touchscreen covers:
– Up to two sensor bases with CO2 option
– Up to four sensor bases without CO2 option
• SmartX LCD temperature sensors: Up to four sensors are supported
- Cat 5/6 cable (22 to 26 AWG) terminated via RJ-45.
- 61 m (200 ft.) total maximum length.
Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Range:
Explore more
Category:
Range: