{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the 12U and 18U NetShelter SX cabinets IBC High Seismic Area of OSHPD compliant?
Issue:
Looking for seismic compliance.

Product Line:
NetShelter SX 12U, 28U

Environment:
All versions and serial ranges.

Cause:
I cusotmer is asking if the NetShelter SX 12U or 18U cabinets are either IBC High Seismic Area or OSHPD compliant.

Resolution:

At the current time the cabinets are not OSHPD or IBC compliant.
Compliance is forthcoming, and this document will be updated when compliance is met.

Schneider Electric Saudi Arabia