{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the static load capacity of a NetShelter WX wall mount cabinet?
Issue:
I customer is asking for static load capacity of a NetShelter WX cabinet. It's not noted in the Specification tab on the APC website.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
A customer needs to make sure they don;t exceed the load rating, or that it meets their needs.

Resolution:

All of the NetShelter WX cabinets have a static load rating of 200 lbs.

Schneider Electric Saudi Arabia