{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to keep existing IP54 protection on Altivar ATV650 or Altivar ATV950 if keypad VW3A1111 is removed from Altivar?
In order to keep IP protection on the drive after the keypad has been removed, it is necessary to use blank cover VW3A1116.
Attached pdf shows the details.

Schneider Electric Saudi Arabia

Attachment(s)
ATV_IS_IP55_Blanking_Cap VW3A1116_NVE77178_00.pdf [1.92 MB]