{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the AR9000RAMP reusable? If so, how many times can it be reused?
Issue:
There is no documentation stating how many times the ramp can be reused.

Product Line:
NetShelter SX HS

Environment:
All versions and serial ranges.

Cause:
It is unknown whether the AR9000RAMP is reusable.

Resolution:

Yes, the AR9000RAMP is reusable.
Although there is no set number of times it may be reused, the Installation Manual has the following statement:

Schneider Electric Saudi Arabia