Is is possible to use electronic thermal overload relay between ATS22 or ATS48 and the motor if there are 2 motors in parallel for one ATS?YEs, it is possible to use LR9D or LR9F electronic relays due to fact that the current has line frequency (50 or 60Hz)
Released for:Schneider Electric Saudi Arabia