{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which NetShelter cabinets are compatible with EcoAisle and HyperPod?
Issue:
Not all NetShelter cabinets can install into both EcoAisle and HyperPod.

Product Line:
NetShelter SX, VX Seismic, SV

Environment:
All versions and serial ranges.

Cause:
We need to prevent a mismatch between aisle containment and the cabinet used.

Resolution:

EcoAisle is designed to be used with NetShelter SX cabinets.
HyperPod is designed to be used with a wide variety of cabinets, NetShelter and 3rd party.

Schneider Electric Saudi Arabia