Search FAQs
what is the reason of Reset Reason 8 in Scada pack ER Magna RTU ?
A reset reason of 8, simply means that someone or some code triggered the SCADAPack to restart. You can do this in Configurator by selecting the dropdown menu "Commands -> Restart RTU ...". It can also be performed via command line interface by typing "Restart RTU"
If a user wanted to program the SCADApack to do this in logic it could also be possible with the "cmd_exec" function block, where the block has the input iCmd as 'Restart RTU".
ClearSCADA can also issue commands like this.
If a user wanted to program the SCADApack to do this in logic it could also be possible with the "cmd_exec" function block, where the block has the input iCmd as 'Restart RTU".
ClearSCADA can also issue commands like this.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: