{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which EcoStruxure Building Operation objects can custom types applied to?
Custom types save time when you have to update a lot of objects that are basically the same regarding their content and structure. You change one custom type and then all the instances attached to that custom type are changed at the same time.

The Custom Types feature consists of two parts: a custom type and one or many instances attached to the custom type. Using the custom type, you can edit many instances at the same time.

The custom types feature is applied to the following objects and applications in EcoStruxure BMS:
  • Graphics
  • Function blocks
  • Script programing
  • MP Series controllers
  • RP Series controllers
  • SE8000 devices
  • Application folders
  • Segments

Schneider Electric Saudi Arabia