{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use TeSys island in a Ring Topology?
Issue:
Does TeSys Island support ring topology

Product Line:
Tesys Island

Environment:
Digital multifunctional load management solution

Resolution:
Yes, RSTP is enabled by default when storing a configuration from the DTM. Make sure to use the 2 fieldbus ports, as it is not enabled for the top Service port.

Schneider Electric Saudi Arabia