Issue:
Programming ATV320 to coast to stop rather than a controlled stop
Resolution:
ATV320 default stop is ramp stop. When you need the motor to coast to stop instead of ramp stop, adjust parameters as follows. Navigate on the display to ConF > FULL > Fun > Stt- > Stt. The factory setting is rMP, change this to nSt.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Saudi Arabia