{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why Control Expert does not show Derived Data Types for devices added on DTM Browser?
Issue
When a user configure a DIO (Device IO) on a DTM Browser of a M580 application, the variables do not show as Derived Data Types as it used to be on M340 and Quantum applications.

Product Line
Control Expert, M580, M340, Quantum

Environment
Control Expert v14.0

Resolution
In M340 and Quantum applications the Control Expert software converts the EtherNet/IP or Modbus configuration data to variables and derived data types from the Input area and Output area. In a M580 application the Control Expert software directly creates a Device DDT.
Below is described the definition of the two different mapping rules and where they are located on Control Expert project.

Derived Data Type family (DDT)
The DDT family includes "derived" data types such as:
  • tables
  • structures
DDT Family
Project browser

Device Derived Data Types (Device DDT)
A Device DDT is a DDT predefined by the manufacturer and not modifiable by user. It contains the I/O language elements of an I/O module.

Derived devices
Derived tables

As a reminder, any variable can be reorganized using the "Alias of" feature.


Schneider Electric Saudi Arabia