Search FAQs
What is the current state 0 guaranteed for BMXDDI3202K?
Issue
The datasheet of BMXDDI3202K and the Control Expert v14.0 documentation do not have the same value for the current state 0 guaranteed for this module. This FAQ shows the right value to be used by the customer while doing specification of devices to be connected on this module.
Product Line
Control Expert, BMXDDI3202K
Environment
Control Expert v14.0, BMEP584040, BMXDDI3202K
Resolution
The IEC61131-2 standard defined the IEC Type and this standard is used by Schneider Electric's PLC products. The BMXDDI3202K is compliance with IEC61131-2 Type 1 and the current at state 0 is < 0.5mA as described on the documentation of Control Expert v14.0.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009P4YKQA0&oid=00DA0000000abSm)
P.S.: Schneider Electric is currently updating all the documentations of this module with the right information.
The datasheet of BMXDDI3202K and the Control Expert v14.0 documentation do not have the same value for the current state 0 guaranteed for this module. This FAQ shows the right value to be used by the customer while doing specification of devices to be connected on this module.
Product Line
Control Expert, BMXDDI3202K
Environment
Control Expert v14.0, BMEP584040, BMXDDI3202K
Resolution
The IEC61131-2 standard defined the IEC Type and this standard is used by Schneider Electric's PLC products. The BMXDDI3202K is compliance with IEC61131-2 Type 1 and the current at state 0 is < 0.5mA as described on the documentation of Control Expert v14.0.
P.S.: Schneider Electric is currently updating all the documentations of this module with the right information.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: